Menus and Toolbar Overview
The KAS IDE
"Integrated development environment"
An integrated development environment is a type of computer software that assists computer programmers in developing software.
IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger contains the five following menus:
...and the following toolbars:
- Tools
- Device
- EtherCAT
- Online Change
- Debug
- Links to the Help and Kollmorgen Developer Network (KDN)
A specific toolbar is also available for the AKD drive.
For details about icons available in the graphical PLC
"Programmable Logic Controller"
A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines.
Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events editors, see these sections: